In the data sheet of TPS62122, there says Output Current is 75 mA.
I have two questions for this output current.
1. Is this mean TPS62122's maximum capable current is 75mA? What happens is loader takes more current than 75mA? Then IC can be damaged?
2. Normally, I learned when choosing buck converter's inductor, normally about 30% delta of Iavg.
If TPS62122's max capable current is 75mA, then is this mean I should choose Avg.current for 60mA System? (60mA * 30% delta = 78mA(about 75mA))
Or can I use 75mA for Average and peak current for 100mA (75mA * 30%) ?