Part Number: LM5155-Q1
Other Parts Discussed in Thread: LM5155
Hi Team,
I have questions about UVLO/SYNC pin specifications as below.
1. Do we have any spec for current flow at UVLO/SYNC pin? I can only find <1mA recommendation when UVLO/SYNC pin is driven by MCU directly.
2. Is that typo?
D/S p.19
"Also, in this configuration, it is recommended to apply the external clock pulses after the BIAS is supplied.
By limiting the current flowing into the UVLO pin below 1 mA using a current limiting resistor, the external clock pulses can be supplied before the BIAS is supplied."
Regards,
Kotaro Yamashita