Other Parts Discussed in Thread: BQ24004
Hi.
Refer to the circuit shown in Fig.1 of SLUS025F and change to the following parts.
・ Q1: 2SA2097
・ C1: 10uF × 2
・ RT1: 10kΩ
・ RT2: 39kΩ
・ Rsns, R1, C2 unchanged
・ Battery
Rated capacity: 2800mAh
Nominal voltage: 7.2V
Charging voltage: 8.2V
Charging current: MAX.1400mA
1. What are the conditions for turning off Q1?
2. Does Q1 fit this mechanism?
3.I am trying to change Rsns to 0.1Ω. Does Q1 work properly?
please tell me!