Hi,
1.System used BQ35100 which follow reference design.And BQ35100 TRM suggested load current is 1000mA for current calibration,but system max current is 500mA,Whether the load current can be reduced?If yes,please help to suggested load current.
2.There have two methods to calibration BQ35100,Is there any difference in the values written to the other registers(which except the register shown in below figure)
1.Use Battery Management Studio software
2.Uesd the mothods mentioned in document SLUA665,detail shown in below figure