This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50-R1 recovery query of over current discharge protection

Part Number: BQ40Z50-R1

Hi

The battery is a 3 series lithium battery, which is fully charged with 12.6V; over discharge current test, after OCD protection, cannot be charged.
In this state, cannot use 12.6V to charge or discharge anymore.
The reason as below:
1. The over discharge current protection recovery current is set to 10mA, it needs to be charged to recover;

2. The CHGFET bit is 0, and the charging MOS is not turned off when it is 100% full;

3. After over-current test, the total voltage of the cell is about 12.3V.

4. The charger voltage is 12.6 <12.3 + discharge MOS diode voltage drop (about 0.6V). Therefore, it cannot be charged.
The battery cannot be charged or discharged on the device.
Please give some suggestions for this phenomenon.
Thanks
Star