Hello, I have been working on putting this board together for the last month or so and I just have a few last questions I was not able to find in the gigantic datasheet :)
1. What is the minimum difference between cells to start balancing?
2. I don't understand what load removal detection is and what it is for /when would you enable it or disable it?
3. I noticed some faults don't clear by themselves and require the battery to be removed and reconnected to clear the fault and restart the chip.
a) which faults does this apply to?
b). can you connect a charger to the board to clear the fault instead of removing the battery?
c) is there anyway to not need manual intervention to clear the fault? If not, is there an appropriate spot to put a reset button? (So the end user in a closed system does not have to open the device)
Thanks for answering my questions! I spent a lot of time in the datasheet and was not clear about these 3 things.