This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808: Need more info regarding Vol / Iol over temperature @ Vdd = 3.3V & 5V

Part Number: TPS3808

I have a customer looking into using the TPS3808 for a product.

For their evaluation, they need data regarding the Vol/Iol for 1.8V, 3.3V and 5V over temperature, for 3mA Iol, or for 1mA / 5mA Iol.

. Something like Figure 7 & 8 from the Datasheet if possible, but including MAX for over temp.

Electrical Characteristics in DS has over temp, but only for Iol @ 1mA. Having this for 3mA or 5mA would be perfect...

Any help would be hugely appreciated.

Regards,

Darren

  • Hi Darren,

    It may take some time to provide this data but I would like to learn more about the application and the customer's requirements. What is the end equipment? What is the project schedule? What is the circuit configuration? Can you explain what is connected to the /RESET output?

    Please provide additional details about this product to michaeldesando@ti.com thanks!