Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21521: VDDB UVLO issue

Part Number: UCC21521
Other Parts Discussed in Thread: UCC21520

We use ucc21521ADW to drive a half bridge, VOB for high side MOS with a bootstrap diode as typical application, once we disable the driver by EN pin and then restart the IC, VOB also has a 50us delay to output pulse, although both input VIA and VIB always be there. We measured the waveform of VDDB vs VSSB, the voltage was setup by one switching cycle and the value excess the UVLO_ON threshold. It looks like that  needs a response time to generate the output. How do we avoid this response delay and get the two pulses simultaneously when we release EN pin? 

  • Hi,

    Thank you for your question. I work on the applications team in the high power drivers group.

    As you have seen, UCC21521 has an approximately 50us UVLO turn-on delay. This delay is necessary for the driver to properly start up internal voltage rails and ensure proper operation. Unfortunately, when using a bootstrap circuit, there is no way around this delay, so it will need to be considered at the system level. We have seen many other customers able to successfully implement a bootstrap pre-charge routine, like described in the image below. The other option is to switch to an isolated bias supply, like a flyback or push-pull, which helps power up the device before switching starts.

     

    I see that this delay has been added to the UCC21520 datasheet, which uses the same silicon. I will work to add this start-up delay and further information to the UCC21521 datasheet as well.

    If this answered your question, could you please press the green button? If not, feel free to ask more questions.

    Thanks and best regards,

    John

  • Got it, thanks!