This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25842-Q1: TPS25842QWRHBRQ1 feature

Part Number: TPS25842-Q1

Hi,

could you tell me the TPS25842-Q1 has below feature?

Stand-by current suppression 

External Trigger of Oscillation

Over Current Protection Circuit

Thermal protection circuit

Variable Output Voltage Control

Output Enable Terminal

Soft Start Function

Hiccup Method Current Control

regards,

Suzuki

  • Hi Suzuki-san,

    I think most of the parameter can be find in the datasheet.

    Summary as below:

    Stand-by current suppression --700uA typical value

    External Trigger of Oscillation-- It has the SYNC pin for external synchronize, frequency from 300K to 2.2Mhz

    Over Current Protection Circuit--Device has internal Buck average current limit and external FET current limit  funcition. ILIM pin for the current limit threshold setting.

    Thermal protection circuit--Device internal has the OTSD function, shut down at 160C and recovery in 140C

    Variable Output Voltage Control--Device default output voltage at 5.1V, IMON pin can set the long cable drop compensation

    detail can refer to datasheet page 32 "cable compensation" section

    Output Enable Terminal-- Output is active by the EN pin control.

    Soft Start Function----fix at 4mS soft  startup 

    Hiccup Method Current Control---Once switching current touch the high side current limit  threshold and for 128 cycle, device going into the hiccup  model 

    Pls. let me know if you have more questions.

    Michael