Hello,
I'm planning to connect three solar panels to the one MPPT. Each solar panel will use a some type of reverse current protector connected in a series. The easiest way would be to use a schottky diode, but at higher currents this could lead to relatively high power dissipation. The better variant is to use P-MOS transistor or N-MOS. N-MOS has lower Rds_on in the same case (in compare to P-MOS), but it needs a driver. LM74610-Q1 looks good for this application. But, I'm not sure - if any of solar panel is completly shaded at one moment, and other two panels are normaly illuminated at the same time, could this lead that the reverse current from other two panels will flow in to the shaded panel?- in this example the panel will get negative voltage, but LM74610-Q1 will turn-off N-MOS relatively immediately, am I right?
On the other side...maybe N-MOS with driver is "too complicated", P-MOS could perform task in a simmilar way but with small number of components...
Many thanks for suggestions,
Kind regards.