This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8867-Q1: Is CFB for preventing oscillation of internal amplifier?

Part Number: LP8867-Q1

Hi team, 

Is CFB for preventing oscillation of internal amplifier?

"8.3.1.2.3 Feedback Capacitor" says CFB is needed if fsw is high such as 2.2MHz. I guess it is related to phase compensation, is it correct?
And this is why CFB is not needed if we use fsw=400kHz, is it right?

Regards,
Ochi