This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62160-Q1: Question regarding schematics and PCB

Part Number: TPS62160-Q1


Hello!

My goal of this schematic is to build buck converter from 12-14.4v (4*LiFePO4) to 5V/1A that can be utilized as mobile charger

While i was building the PCB based on datasheet and other study materials, i have completed to build PCB but not sure if this is quite okay to use. So i wonder if you guys can give me feedback on my PCB.

Also, as i run DRC in my PCB, it says my USB port shield should be connected as warning. should i just go over it?

I attatched my schematic as well as PCB design. 

Thank you!