This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: Internal pullup or pull down on Enable pin?

Part Number: TPS2595

Hi,

For the enable pin, is there an internal pull up or pull down on it and if so what is the value?  This reason I am asking is that I am using the active high enable part and have a 10k pulldown to ground.  At power up, before the uC is online, the net is tristated, and the enable pin crosses the enable threshold to turn on the system.  Then once the uC is online, and disables the enable by no longer being tristated, the output goes off as expected.  

Im just wondering if I need to increase the pulldown to 4.7K or 1 k, so any insight into the enable pin would be great.

Thank you,

Will