This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the design for LED driver recommendation

Other Parts Discussed in Thread: TLC5973

Hi Team,

Customer is designing LED driver.

Would you please provide recommendation for the following questions?

 

LED driver IC which is available to package into LED directly, or can be a standalone packaged IC. Attachment is the IC datasheet for reference, pin assignment should be same or similar, and the woking methodology should be exactly the same. 

Besides, there are some requirements needs to be meet.

  • operation current:<0.5mA, the smaller the better
  • sleep mode is preferred
  • maximal driving current: <5mA
  • IC chip size: smaller or similar to datasheet
  • packaged IC size:<2x2mm, the smaller the better

 txn.box.com/.../lif21ryrgldyimwjpm8m4placw7rv2db

BR,

SHH