Part Number: LM2576
Other Parts Discussed in Thread: LMR16020, LMR16030, TPS54560, LM5164
Hello
Step Down regulator with 60V input and output 2 amp.
1- We use IC Lm2576HV. Is there another IC that has better quality and less output noise?
We need an IC with an input of 9 to 60 volts for a 5 volt fixed output with 2 amps.for example; we used 24v in with 5v 2A out and 60v in with 5v 0.5A out.
2- Can we say that the LM2576-5V-fix is better than LM2576-Adj for a constant 5V output? Is there less noise and better quality because the air LM2576-5V-fix does not need feedback resistance?