Hi,
The application we have now for using BQ25713 is as below.
- Max Charge current: 8796mA
- Max discharge current: 8000mA
Based on BQ25713 spec I think we need to use a lower Rsense value between SRP and SRN, so the plan is to use a 5mohm resistor here.
So, our questions are,
- From HW design, what else would be changed to fir 5mohm Rsense?
- From SW register, which register should be configured or decoded in a different way to match 5mohm design?
THanks!
Antony