Other Parts Discussed in Thread: BQSTUDIO
Hello all,
I have been trying to complete a learning cycle using the BQ40Z80 and a 7S2P battery pack (6600mAh).I need that work at 3.05V to 4.15V.I set the design capacity settings (Design Capacity mAh = 6000mAh, Design Capacity cWh = 15120cWh, Design Voltage = 25200mV) The FC Set Voltage Threshold is set to 4150mV. Charge Term Taper Current is set to 1000mA, Dsg Current Threshold is set to 300mA, Chg Current Threshold is set to 500mA, Quit Current is set to 250mA, Term Voltage is set to 21350mV.
Here is a short summary of the procedure:
1. Update the chem id.
2. Send FET enable(0x22)
3. Discharge Battery to Empty and rest 5 hours Until REST = 1.
4.send IT (Gauge) enable command (0x21)
4.Charge the battery to full and wait until FC=1.
Rest 2 hours until VOK = 0,RDIS=0 ,REST = 1.But the Lstatus do not change to 0x05.
why the Lstatus do not change to 0x05???