This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2553: Differences TPS2553, TPS2553-1 und TPS2553D

Part Number: TPS2553

Hello,

Can you please confirm the following two statements?

  1. TPS2553, TPS2553D and TPS2553-1 all have Reverse-Blocking function
  2. The only difference between TPS2553 and TPS2553D is the operating temperature.

Thanks and best regards,

Gökhan

  • Hi Gokhan,

    TPS2553-1 is latch off version. TPS2553 is constant current limit version.

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.

  • Ziv Zhang said:

    Hi Gokhan,

    TPS2553-1 is latch off version. TPS2553 is constant current limit version.

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.

    Hello Zhang,

    Does the TPS2553TPS2553D and TPS2553-1 all have Reverse-Blocking function? I am asking because it is not mentioned on the product page of the TPS2553 and TPS2553-1 but it is mentioned on the TPS2553D product page. The customer wants to have a confirmation. However on the datasheet all seem to have Reverse-Blocking function. Can you just quickly confirm? 

    Thanks

  • Hi,

    Yes, all have reverse block function.

    But please get noted that the reverse voltage protection time to turn off the IC is 5ms(typical).

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.