This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24617: How to avoid entering sleep mode when using 5V adapter?

Part Number: BQ24617
Other Parts Discussed in Thread: BQ25606

Hi Teams,

My customer applies BQ24617 in their project.

The use case is Lithium battery 1S3P with charge voltage 4.35V/ charge current 3A.

They have two kinds of input voltage,12VIN and 5VIN.

When Vin=12V, everything goes well.

But when Vin=5V,  the BQ24617 stop charging until the battery is discharged.

We know that BQ2461X series Vcc must be at least 500mV higher than SRN to avoid entering sleep mode.

Due to the customer must have 5V and 12V input voltage in their application, do you have any suggestions to solve this problem?

If BQ24617 cannot meet this requirement, could you kindly recommend a suitable device for this application? 

Thanks and best regards,

Jamie