This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: TPS92692 output power

Part Number: TPS92692

Dear Sir, please answer

I need LED driver for input power supply 10 - 30 V.

Max output current for TPS92692 is 5 A, max output voltage is 65 V. 

QUESTION: Then I can derive 65 x 5 = 325 W output power?

TIA.

Sincerely,

Vladimir Naumenkov

www.agat.by