Good afternoon....
I have reviewed the datasheet and still have questions......
With respect to the above part:
1. Can you tell me does the Charge Timeout work on the Constant Current phase only or over the whole cycle? I am confused as to how to tie the TTC pin and whether or not to place a capacitor there for charge timeout....
2. What is the difference between Charge Timeout and termination?
3. Also I have set the Iset1 to 7.875A...The load may draw up to 3.5A....The part mentions that it is capable of charging up to 10A....Is it safe to say that the load current is NOT part of this 10A path? ...and secondly is it safe to say that if I place a low inductance in there (say 4.7uH) such that I have a ripple current of 4A which yields a peak of 12A on the battery charging side that I will be safe to not damage the part?
Sincerely,
Steve