This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: About reverse polarity protection on UVLO pin

Part Number: TPS2660

Hello,

 

Regarding to reverse polarity protection on TPS2660, my customer is asking a question.

According to datasheet page 21, reverse polarity protection is described as following.

“In the applications where reverse polarity protection is required connect a minimum of 300-kΩ resistor between UVLO and IN_SYS.”

 

(Question)

Could you please tell me why 300-kΩ resistor can protect to reverse polarity( min -60V)?

(The reason of why the resistor is 300kΩ minimum.)

 

Regards,

Tao_2199

  • Hi Tao,

    UVLO is rated to -0.3V on the negative side. So, min 300kOhm is recommended to protect UVLO pin under reverse polarity condition.

    Best Regards, Rakesh

  • Hello Rakesh.

     

    Thank you for reply.

    I have additional question.

     

    ・Why 300-kΩ resistor can protect from -0.3V(UVLO minimum rate)?

    Does this device protect UVLO pin by internal protect diode?

    Or is it related with UVLO Input leakage current?

    Could you please tell us theoretical explanation more detail?

     

    Regards,

    Tao_2199

  • Hi Tao,

    As you know, each pin has ESD diodes. These diodes get forward biased under reverse polarity condition and excessive currents could flow leading to the damage. To avoid that, -0.3V limit is imposed in the spec. The other way is to use a resistor in the path to limit the currents (under few mA) through the ESD diode under reverse polarity condition. This is what the 300-kΩ resistor does here.

    Best Regards, Rakesh