This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: BQ34110 register

Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO

dear 

1. In the BQ34110RM manual, it seems that the operation is written through the Control command word to achieve the effect of different configurations. However, I have seen that there are 57 relevant configurations.and how about common initialization configuration?

2. According to the document, it is written by two-byte command, and an instruction needs to be transmitted twice.Take Control_Status in Control() as an example, whose CMD Control word is 0x00\0x01 and DATA content is 0x0000, whether to write high byte or low byte first?

3. In terms of Pin Control config, it is through the configuration of Alert1_x_config, Alert2_x_config to achieve the functional goal, how to configure?Can multiple trigger events be configured with the same pin?How to distinguish between multiple trigger events when configured.

4. It is Required for applications of more than one-series cell.Otherwise, BAT connects directly to single - cell BAT + and VEN can be left unconnected, if voltageno more than one

Set value,can  connect the power supply directly?What is the set value?

thanks in advance