hi,
in the bq24707a, I have set input current register 0x3f to numerous current levels, including 128mA, I have set 0x12 to 0x218 which should enable Acoc function. no matter what I do, either set my charge current more than 2x above my input current, or draw additional current from acn to gnd using a resistor, the ifault does not trip.
I also do not understand "the ic cannot maintain the input current level if the charge current has been already reduced to 0" does this mean I have to have my charge current be 0, and draw current through the acp acn shunt externally to trigger the ifault? either way, I could not trigger a fault.