Other Parts Discussed in Thread: BQ76930, BQ78350, GPCCEDV
Hi,
I am using BQ76930 and BQ78350 for my battery pack. And I will use CEDV function but I have issue about the log files which I have to upload GPCPackager for CEDV fuction.
I will use my battery from -20°C to 30°C. And my load is not constant.
Which 3 temperature level should I apply ? I am thinking to apply -20°C, 10°C and 30°C.
My repeater load profile is;
300W | 100ms |
150W | 500ms |
200W |
40s |
150W | 10s |
50W | 5s |
This load profile repeats until SOC gets down %0.
I need to apply 2 load profile for CEDV. Should I apply half and full of this profile values?