This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61087: value of Rcomp

Part Number: TPS61087


Dear all,

Our customers rate TPS61087 under the following conditions:

  • Vin = 4V
  • Vout = 8V
  • L = 6.8μH (Fsw = 650kHz)
  • Cout = 44μF
  • Rcomp = 7.5kΩ
  • Ccomp = 2700pF

When I calculated Rcomp and Ccomp under the above conditions to check the circuit, the results were as follows.
* Calculation formula was as described in the data sheet

  • Rcomp = 22.776kΩ
  • Ccomp = 2061pF

Especially, the value of Rcomp is much smaller than the calculated value.
Does this have any operational problems such as device responsiveness?

Best Regards,

Y.Ottey