This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: Absolute max for current

Genius 17635 points
Part Number: TPS22810


Hello,

There is not information about absolute max current in the TPS22810 datasheet(SLVSDH0C).
What is the absolute max current value?

Regards,
Oba

  • Hi Oba,

    The maximum recommended current values for the TPS22810 would be 2A, and 3A for the DBV and DRV packages respectively. We cannot guarantee safe operation of the device with currents higher than the above mentioned.

    Best regards,

    Andy Robles