Hi,
My backup power uses 2 series supercapacitors (2 x 350F 2.7v = 5.4v)
I need to modify the design in order to add a fast discharging circuit.
The discharge should be fast and safe. (less than 2-3 min).
The switching during normal use (charge and powering) is managed by a LTC3226.
Is there any IC that I can add in order to switch on fast discharge ?
Thanks