Other Parts Discussed in Thread: TPS61022
Hi Team,
When looking at the TPS61023 datasheet, there are two conditions for what frequency to select the Cff value to make a zero frequency (pasted below):
For large output capacitance more than 40 μF application, TI recommends a feedforward capacitor to set the zero frequency (fFFZ) to 1 kHz. As for the input voltage lower than 1-V application, TI recommends to use the effective output capacitance is about 100 µF and set the zero frequency (fFFZ) to 1 kHz.
Are both of these supposed to be 1kHz? When looking at the TPS61022 datasheet it has a similar statement but with two different frequencies, see below:
For large output capacitance more than 40 μF application, TI recommends a feedforward capacitor to set the zero frequency (fFFZ) to 2 kHz. As for the input voltage lower than 2-V application, TI recommends setting the zero frequency (fFFZ) to 20 kHz when the effective output capacitance is less than 40 μF.
Thank you!
Reed