I have designed a 9 cell Battery Pack using the bq76930. It pretty much works except I am running across one problem. Cell 9 will charge faster (3 different battery packs). I can see the bleed resistor turn on (100 ohms) when it tries to balance and the cell 9 doesn't seem to care it just keeps charging. I tried 50 ohms too. This is the last cell in the pack and I know there are a few items that must be taken care of to make it work. I am using the EM as a design reference. I have removed the cap between VC9 and VC8 and replaced it with a 0 ohm resistor, I have removed R23 and R33, I have shorted C9 and C8 together and have cell 9 connected between C8 and C10. Most of the cells get to 3.35V to 3.36 and stop, but cell 9 will go up to 3.6 where the Micro will stop the charging. Am I just trying to over charge the cells? LiFePo3 A123 2665. Nominal is 3.3V Charging Voltage is 3.6.