Other Parts Discussed in Thread: BQ34110, BQ34Z100
Dear team,
our customer is developing his own battery pack based on 5S NiMH cells. The battery cell planned is VH1800AA. They selected BQ34Z100-G1
The customer told me they did not receive the chemistry files from the cell manufacturer and will have to create their own golden image file. (Or can we look up this type of battery in BQ Studio?) The customer is wondering if there was training material he could follow to do create the golden image.
He would also want to have design reviewed. I do have the schematic and battery information under NDA but this needs to be done offline. How can we do this?
Would BQ34Z100-G1 be the best part or should they move to BQ34110 or some other part? There will be a MCU in the pack as the customer has his own LED indication scheme - so no use of the LED feature of BQ34Z100-G1.
many thanks
Lutz