Hi Team,
Customer is designing new project with power switch
Would you please provide recommend the p2p solution to replace the following two parts?
- G517D1T11U
- G524B1T11U
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi SHH,
Welcome to E2E!
We do not have P2P solutions for these devices, but have some devices that offer similar functionality.
The G517D1T11U and G524B1T11U are both devices with reverse current blocking and over current protection. These functionalities are offered in the TPS22948, but the TPS22948 can only handle 240mA typical. We also have the TPS22919 which offers short circuit protection, but does not have reverse current blocking.
What are the key specs that the customer likes from these two devices?
Best regards,
Andy Robles
Hi Andy,
thanks for feedback.
customer design this in the USB port for OCP protection.
BR,
SHH
Hi SHH,
I will be re-assigning the thread to a team I believe would have similar devices to the ones you mentioned. Someone will get back to you shortly.
Best regards,
Andy Robles
Hi SHH,
Please check TPS25221.
For G524, can you help tell me the package?
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.