Other Parts Discussed in Thread: TPS40322, , TPS51604
Hello,
In the recommended applications there is a driver IC shown next to the CSD86360Q5D. Does TI have a device that fits this roll that can be powered by a 3.3V PWM signal? The reference design has uses the TPS40322. However the application has us using a particular Infineon controller, as the load is an AMD SVI2 based processor. The controller outputs a 3.3V PWM signal that our "Driver IC" would convert to the upper and lower gate controls.
Essentially the sample TPS40322 device is too complex and we need a simpler gate-driver circuit, an 8-pin device like what is shown in the datasheet would be excellent.
Thanks,
Talon