Dear Sir,
I have a project need 1000 lm or more.
My setting conditions are as follows:
LED : OSRAM LED (Vf 2.7V-3.0V / If 700mA ).
LED Q'ty : 4 pcs LED / 1 serial (the voltage is 10.8V-12V and the current is 700mA).
Power : Li-poly battery (3.7V / 5000 mA).
Dimming : PWM signal from Arduino.
If I use LM3410 to drive it, is it ok ?
If not, please give me some suggestion.
Thank you.