This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50_R1 SOC problem

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQSTUDIO

       We Use BQ40Z50R1 for 4s LifePO4,After aging, our battery has a charge of 80%, but after standing for a period of time, the SOC of some batteries will become 95%, and some will become 75%, most of which are 80%, and the problematic ratio is 20%. We made ID and mass production documents according to the requirements。What is the problem and how to solve it?

       We make the ID on GPC ,our ID is 457: DOD error is 7.44%.