Other Parts Discussed in Thread: TPS65131
Hi Team
Would you advise my customer's question of Vneg max current at
Vin = 3.15V, Vout = - 6.7V?
Because max current is difficult to estimate from the below graph in datasheet.
Thanks
Best regards,
Shidara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have notified our expert regarding this topic. Please expect a response by 4/23/20.
Thanks,
Aaron
Hello Shidara-san,
Maximum load current is dependent on input voltage, output voltage, load current and converter efficiency. Basically, in the case of TPS65130/131 it is limited by internal switch current limit. Theoretical max current at Vin=3.15V, Vout=-6.7V should be ~160mA for TPS65130. If customer is concerned about max current margin, I would suggest to use TPS65131 instead of TPS65130 because it has a much higher internal switch current limit and hence can support much higher load current.
Kind Regards,
Liaqat
Hi Liaqat-san
Thank you so much for your advice.
If I choose TPS65131, Theoretical max current will be 399mA, right?
Any advice should be highly appreciated.
Thanks
Best regards,
Shidara
Hi Shidara-san,
For TPS65131, theoretical maximum current with conditions provided will be approx. 450mA.
Kind Regards,
Liaqat