Tool/software: WEBENCH® Design Tools
Hello,
I have simulated a converter with WEBENCH, I have attached the simulation.
The inductor suggested is a DRQ127-3R3-R, datasheet report for the series configuration a max Irms = 5.23 A and Isatpeak=10.8A. looking the graphics for Lin (see below) it seems that the current can be higher than 5.23A.
Are my considerations wrong ? Can I use that inductor even if Vin=4V and Iout = 3A, as required in my simulation ?
Best regards
Riccardo