Part Number: BQ27750
Dear TI, I use BQ27750 for 36Ah battery ( 4 Ah*9 Cells ). For FCC and RM registers limit is 32767. As result of this I need calibrate current like 1:2 ( real : variable ). Means +1 A charge shows on BQStudio like +500 mA. At first, I was charging the battery until full charge statement, and then start discharge with constant current -1A ( for microcontroller -500mA ). At the end of the test (after 35h.) I compare result from discharge machine and from BQ27750. Discharge machine shows 35 Ah. But on the BQ27750 ( if calculate: RMCapacity_0h – RMCapacity_35h ) = 16.2 *2 = 32.4 Ah. If I manualy intergrate data CoulombCounter from BQStudio, I have the same result like discharge machine 17.5*2 = 35 Ah! Correct value!
Means, measuring CoulombCounter of BQ27750 is perfect. Also Qmax Cell1 calculation is correct.
But Impedance Track algorithm calculation of RMCapacity is wrong ( also FCC after updating ).
I make that test at two types of discharge machines with few a batteries at min. 4 cycles – the same result.
And my question – what can be wrong at ITrack settings?
From «Theory and Implementation of Impedance Track Battery Fuel-Gauging Algorithm» document I can see BQStudio «indirectly» measuring internal resistance of battery, but there is not information how? If R = deltaU / I, BQ27750 ITrack algorithm «doesn’t know» about scaling factor of current and calculate internal resistance ( impedance ) is wrong. As a result is not correct correction of capacity.
Does this sound like the truth?
Best regards, Danil