Hi Team,
As title , my customer is surveying the solution as subject for server system application , the spec as below
There are two 12 or 48V adapters provide power into system, and customer want to balance these two adapters loading.
Adapter 1: 280W, 12 or 48Vout ±5%
Adapter 2: 280W, 12 or 48Vout ±5%
System: 450W, 48Vin or 12Vin
customer original used LTC4370 in as previous project's solution , the previous system adapter is 12Vin,
for the new project in needed to support 450W in total , and the Vin might be 48V,
Please kindly help to suggest the solution if we have any, 12V or 48Vin are both ok, thanks!