Other Parts Discussed in Thread: UCC24650
Hello,
I'm currently trying to implement the UCC28730 circuit in to the a TI reference design 40V-1000Vin 15 Vout but modified to 24 V output instead. I have changed resistor values to match the datasheet of UCC28730 but it won't start switching when I connect 300 V to HV. I saw that VDD needs to be 21 V to keep the switching going after startup. But it seems like the controller don't start switching at all so it won't give a VDD voltage from the AUX on the transformer.
I was reading on a troubleshoot document (http://www.ti.com/lit/an/slua783/slua783.pdfAlso, do I have to use the wakeup circuit UCC24650 to be able to use UCC28730?
Because I am working with a company on my bachelor thesis on this I don't know if I can share the circuit here on an open forum. Any help would mean very much!
Best regards
David