Hello,
I have 2 questions regarding the Qmax after the learning cycle:
1. As in the title, I noticed that the Qmax Pack is the same as Qmax Cell 1 and 2 after the learning cycle. Isn't it should be the sum of Qmax Cell 1 & 2? Is there anything I did wrong here?
2. The Qmax Cells after the learning cycle is about 15% higher than the design capacity of the battery. Is that normal?
Thank you!