Other Parts Discussed in Thread: BQ25703,
Tool/software: WEBENCH® Design Tools
BQ25703 design issues:
1. Can the maximum input current of BQ25703 be set to 6A? We can only input a maximum current of 4A, and cannot increase the input current.
2. Can BQ25703 achieve the following process:
(1) Adapter 12V is connected to the system, when the battery is not connected, VSYS needs to output 12.6V / 4A;
(2) Adapter 12V is connected to the system, the battery (3 batteries in series) is also connected to the system, VBAT charges the battery (charge Current 2A, the battery does not supply power to the load), and VSYS supplies 12.6V / 4A to the load;
(3) The 12V power of the adapter is cut off, and the load is powered by the battery.