This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3809-1: diode selection question in flyback slua086 (U-165)

Genius 3900 points
Part Number: UCC3809-1

Hi there,

I am learning TI slua086 , p7-8 talks about three parameters to consider on diode selection in flyback. I have some questions to consult.

(1) Quote page8 "The peak repetitive forward current is equal to the reflected primary peak current. An MBR2535CTL" . I think when the diode conducting, primay side mosfet is OFF and there should be no primary current, therefore where the "reflected primary peak current" comes from? I am confused.

(2) some notes said Trr (reverse recovery time) is also important for flyback didoe, but it seems not mentioned in diode section of thi paper. Would TI has any advice ?

Thank you!

  • Hello Yi

    1/ "The peak repetitive forward current is equal to the reflected primary peak current" and you are of course correct that the two currents do not flow at the same time. Let's say you have 1A peak current in the primary, then the secondary current would be 1*Np/Ns.  Here's a diagram - showing a typical primary waveform (blue) and a secondary one (red) - the duty cycle is about 50% and the turns ratio is 2:1 so the secondary current peak is twice that of the primary.

    Regards

    Colin

  • Thanks Colin, I understand.  By the way, do you have any advice on my question 2 ? 

  • Hello Yi

    My apologies - I missed that one.

    The reverse recovery of the diode comes into play when the MOSFET is turned on and the diode current drops to zero while the MOSFET current increases - at the time arrowed below.

    It's all very difficult to analyse fully but the basic message is that 'Faster is Better'. When the MOSFET turns on the voltage on the diode reverses. The diode will conduct in the reverse direction for a little while. The losses associated with this can be significant because the reverse voltage across the diode is high.

    So - 'Faster is Better' - typically one would use so-called 'Fast' or 'Ultra Fast' diodes as the 'default' option (trr < 50ns). At low output voltages Schottky diodes are a good choice - like the MBR2535CTL device you mentioned. The reason is that they are majority carrier devices with very fast reverse recovery.

    At high voltages you can consider wide bandgap devices like SiC

    Regards

    Colin

  • Hi Colin, thanks for helping us on this forum for more than once .

  • By the way , should you have spare time, would you please help take a look at this thread on my confusions about flyback mosfet drive peak current, and maybe share some of your insights? Thanks again.

    https://e2e.ti.com/support/power-management/f/196/t/898815

  • Hi Yi

    We can deal with the query about gate drive peak current in the other thread so I will close this one.

    Regards

    Colin