Other Parts Discussed in Thread: TPS56339
Hi,
Kindly please help to advise as I am currently facing high heat issues during switching on the TPS62135, the temperature rises continuously until it cuts off and it's around 120degC. Below are the operating requirements.
Vin: 13.5V
Vout: (application is USB type C charger)
12V 1.5A, 9V 2.0A, 5V 3.0A
Please help to advise on the design improvement which is needed to bring down the heat.