This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HB08-Q1: 24V Operation

Genius 4840 points
Part Number: TPS1HB08-Q1

When my customer use TPS1HB08A-Q1 in 24V VBB operation,we found following description in datasheet.

VBB Extended supply voltage(2)                         3 - 28 V

(2)Device will function within extended operating range, however some parametric values might not apply

Do you have any parameter list at 24V operation.

 

regards,

  • Hello Kura-san,

    Above the 18V nominal operating voltage if a short-to-ground fault occurs the device is not guaranteed to survive. Additionally the only parameter that is specified above 18V is the  on-resistance. Other parameters are only specified VBB = 6 V to 18 V.