This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62260-Q1: Why 2 package schematics?

Part Number: TPS62260-Q1

Hello,

There are 2 package schematics for SON in the datasheet. DRV0006A and DRV0006D. Why 2? And which package is for which product?

Thanks!

Regards,

Oguri (TIJ automotive FAE)

  • Hi Oguri,

    Both packages are the same there is no difference from a technical point. 

    DRV package drawing is for the WSON package and the DDC package drawing is for the SOT23 package.

    Best regards,

    Tanvee

  • Hi Tanvee,

    There is obvious difference between them.

    Please make it clear which one of the packages is for each of the below devices. The customer will examine the devices when they receive to confirm if the correct ones are delivered. When they are found different, they will be rejected. Currently there is no information to determine which one of them is for each device. The information they are technically the same is meaningless here. The difference is obvious.

    Thank you.

    Regards,

    Oguri

    ・TPS62260TDRVRQ1
    ・TPS62262TDRVRQ1

  • Hi Oguri,

    I am discussing it with the packaging team and will get back to you by next week.

    Best regards,

    Tanvee 

  • Hi Oguri,

    DRV006D is correct package drawing for TPS62260-q1 and I will request for the modification of datasheet and another drawing will be removed. Thanks, for pointing it out to us.

    Best regards,

    Tanvee