This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV700: Reverse current issue

Part Number: TLV700

Hey E2E

I have a situation where a battery is directly tied (with a MOSFET in series, to prevent charging) to Vout of the TLV700. Normally a 5V PSU is tied through a diode to V_in of the LDO, but in this test there is no input source.

So when I attach this battery to V_out I see 40mA going into the LDO. I tried pulling CTRL of the LDO down, and it got me to 30mA. According to my measurements all the current is flowing in the LDO only, since I have isolated the circuit from the other parts. 

I am using a keysight N6705C for the current measurements.

Is this normal behaviour? I placed a diode in series with the LDO to avoid back current - but I did not anticipate the LDO to drain all this current by itself!