I want to use the TPS55165Q1 IC with the following settings:
1- Normal Mode ( Always ) with output 12v fixed.
2- Power latch on ( always on even if battery voltage drop during crank ) , without external micro-controller signal if possible . using a pull up or pull down is preferred .
3- with Spread-Spectrum enabled to reduce EMI .
Problem 1: I have problem understanding how to connect IGN_PWRL
IN TPS55165Q1-EVM (SLVUAY1) The schematic shows that inorder to enable the Power latch , the jumper should be connected to GND.
while in datasheet it says in the pin description of IGN_PWRL:" Logic-level IGN power-latch signal. The IGN pin is latched when this pin is high (1) and is not latched when this pin is low (0).
So what is the correct way of connecting this pin ?
Problem 2: SS_En
The datasheet and EVM document states that: This feature can only be enabled when the device is in normal mode with step-down operation.
So if i leave this pin unconnected ( SS enabled )
Does this means that during operation in boost mode ( Vin < 12v) this feature is disable automatically and the device continue working normally ?
Or Does it mean that when operating in boost mode ( Vin < 12v) this device will be disable because SS is enabled ?