Other Parts Discussed in Thread: TPS63802, TPS63806
hi,
i have the following buck -boost requirement
Vin = 4.5 to 5.5 V
Vout=5V
Iout 3A.
can i use the part TPS63020 with 1uH inductor?
if not kindly suggest me a solution
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Milos,
Thank you for the prompt response.
3A is continous.
Datasheet of TPS63020 says it supports 4A of switching current. Hence it is supposed to support 3A of load current right? Correct me if i am wrong.
i have also checked the datasheet of TPS63802, which says it will supports upto 2A.
can you please confirm?.
it would be helpful if you confirm me a part for my requirement
Hi Sajna,
It depends on the device how the switch current limit translates to the maximum output current. The TPS63802 is a newer device, with a higher switch current limit, lower switch Rds,on and better thermal properties than the TPS63020. The TPS63020 cannot support the continuous output current shown in its datasheet in Figure 1. The TPS63802 can support continuous output current shown in its datasheet in Figure 14. However note that this is measured on the TPS63802 EVM at room temperature and with the recommended layout.
The TPS63806 can support a bit more current, but it comes in a BGA package.
Best regards,
Milos
hi Milos,
what would be maximum current TPS63020 would support for 5V output
Input is in the range 4.5V to 5.5V.
im in the middle of my design with TPS63020 for 2.7A output. Shall i proceed? or need to switch my design to TPS63806?
Regards
sajna