Hello,
I have a couple of questions about TPS543C20A as follows.
Q1:
Datasheet says KIND must be kept between 0.1 and 0.3 for balanced performance.
However, KIND can be 0 – 200% at WeBench.
If KIND is > 0.3, for example KIND is 2.0, what would be wrong?
Q2:
IOCP is defined as the valley inductor current?
So, actual maximum DC current limit is IOCP + 1/2*(Inductor current ripple)?
Best regards,
K.Hirano